Whitepaper: Testing of HFC Fluids on Common Seal Materials in High Temperature Applications

As the oil and gas industry moves to recover more challenging reserves and enters the development of High Pressure High Temperature (HPHT) fields, the risk of fire is increasing. There is therefore a move to the use of water-based hydraulic fluids, which present significant sealing challenges. 

To ensure sealing performance is maintained in water-based hydraulic fluids, it is imperative that operators understand the effects of high temperature exposure of sealing materials within water-based hydraulic fluids. Until now, these two elements have not been thoroughly tested together at high temperatures.

Download our free whitepaper to learn about: 

The compatibility of seals with HFC fluids
Basic overview & sealing requirements of water-based hydraulic fluid
Specifying & using water-based hydraulic fluid
Testing parameters and results of HFC fluids

© Trelleborg Sealing Solutions